This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sample C\C++ code for controlling the DLP4100



Hi

Can someone send me example C or C++ code for controlling the DLP4100 DMD using the DDC4100.ocx files (or the other dll files)?

Specifically I need C or C++ code that takes a 2D array (like a image) and displays it on the DMD.

We currently have access to the DDC4100.ocx file, but we have no experience handling such types of files in C or C++.

(Yes we tried a MATLAB request earlier but we are desperate and will for C\C++)

Thanks in advance.

-Phill

  • Hello again Phillip.

    You can request C++ sample code for the D4000 kit from the design house that you purchased your D4100 kit.  You will simply need to change the references to D4000 OCX or DLL to D4100, but it will show the right command sequence to display your image.

    Let's see if anyone else out there has already built C++ or MatLab code for the D4100.

    Fizix