Hi, I am trying to set up an experiment using DMD development kit. Since I am hoping for a quick turnaround time, I am very interested in either light commander or light crafter. But one concern I have is that I will need to use external monochromatic laser source, with fairly high power (CW ~0.3W, or pulsed laser with 4ns pulse width and ~kw peak power).
I am wondering if either of these system may sustain such power? Also will it be easy to coupling external laser sources for illumination?
Thanks in advance.