This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DMD* FREQUNCY OPERATION

Guru 13485 points
Other Parts Discussed in Thread: DLPC200

What is the limitation for the opertating frequency?what will happend if we will use higher data rate?

  • Eli,

    Our apolgies that this question got overlooked. 

    Could you clarify which platform you are referring to?  (i.e. D4100, DLPC200, LightCrafter).  For example, the D4100 platform is only specified up to 400 MHz clock.  Above that frequency the PLLs in the controller are not guaranteed to work.

    Fizix