This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Operation with one led in lightcrafter sysytem



I would like to operate a lightcrafter sytem with one led.

Led driver circuit should be chanded for lightening one led full time.

What change will be required?

Please advise me!

Thank you. 

  • This can be done by feeding the same LED at all 3 sequences.   The connection can be modified and current levels can be configured to ensure that a single LED will cover the entire color sequential operation.    Another option is to externally feed the LED you wish to use each time at a certain preset current level while using the original lines for trig purposes.

    We as a DLP design house can provide you assistance or a complete solution.

    Feel free to contact us.

    Yuval

    EKB Technologies, a DLP Design house

    www.ekb.co.il