Other Parts Discussed in Thread: DLPC200
Hello
i have a self-designed DLP board ,
( i bought a LightCommander , so it gave me a lot of help during designing the pcb board)
Now , i have some problems in using my own board:
the run log shows many error when i run the project
Here is the whole run log
#================================================================= # Configuration Registers/LUTs for DLP LightCommander #--------------------------------------------------------- # Created on: Fri Jul 20 10:54:06 2012 # Created by: Texas Instruments DLP Seq Compiler DLL # Version#: 1.5.0 # # Output Attributes: # Comment = NewProject3.lcp New Solution # DMD = XGA # Mode = SL # Display Pattern Frm Rate = 60 Hz # Exposure Time = 16000 usec # Exposure Time/Frm period = 0.96000 # Num BPP: = 1 # Num Patterns in Seq = 1 # Real-time input source = false # Active LEDs = GLED #================================================================= ERROR - USB communication timed out # ExecutePassthroughDLPAPI: Function did not return STAT_OK # Error: unable to execute "$L2.5 ExecutePassthroughDLPAPI _DisablePwmSeq" $L2.5 DLP_RegIO_BeginLUTdata SEQ_LUT $L2.5 WriteReg 0x1111, 0x000000c0 $L2.5 WriteReg 0x1111, 0x00000008 $L2.5 WriteReg 0x1111, 0x00260005 $L2.5 WriteReg 0x1111, 0x00080004 $L2.5 WriteReg 0x1111, 0x00080004 $L2.5 WriteReg 0x1111, 0x00080004 $L2.5 WriteReg 0x1111, 0x00080004 $L2.5 WriteReg 0x1111, 0x00080004 $L2.5 WriteReg 0x1111, 0x00080004 $L2.5 WriteReg 0x1111, 0x00080004 $L2.5 WriteReg 0x1111, 0x00080004 $L2.5 WriteReg 0x1111, 0x00080004 $L2.5 WriteReg 0x1111, 0x00080004 $L2.5 WriteReg 0x1111, 0x00080004 $L2.5 WriteReg 0x1111, 0x00080004 $L2.5 WriteReg 0x1111, 0x00080004 $L2.5 WriteReg 0x1111, 0x00080004 $L2.5 WriteReg 0x1111, 0x00080004 $L2.5 WriteReg 0x1111, 0x00680004 $L2.5 WriteReg 0x1111, 0xa030000a $L2.5 WriteReg 0x1111, 0xffff0003 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x752e0004 $L2.5 WriteReg 0x1111, 0x00300004 $L2.5 WriteReg 0x1111, 0x00000001 $L2.5 WriteReg 0x1111, 0x00180005 $L2.5 WriteReg 0x1111, 0x00f9f004 $L2.5 WriteReg 0x1111, 0x0e669004 $L2.5 WriteReg 0x1111, 0x002f9008 $L2.5 WriteReg 0x1111, 0xc78e9404 $L2.5 WriteReg 0x1111, 0xc78e9404 $L2.5 WriteReg 0x1111, 0xc78e9404 $L2.5 WriteReg 0x1111, 0xc78e9404 $L2.5 WriteReg 0x1111, 0xf9908404 $L2.5 WriteReg 0x1111, 0xf9908404 $L2.5 WriteReg 0x1111, 0xf9908404 $L2.5 WriteReg 0x1111, 0x0f900404 $L2.5 WriteReg 0x1111, 0x00180004 $L2.5 WriteReg 0x1111, 0x00000001 ERROR - USB communication timed out # LC_DLP_RegIO_EndLUTdata: Function did not return STAT_OK # Error: unable to execute "$L2.5 DLP_RegIO_EndLUTdata SEQ_LUT " ERROR - USB communication timed out # WriteReg: Function did not return STAT_OK # Error: unable to execute "$L2.5 WriteReg 0x2B8 0x3f0f" ERROR - USB communication timed out # WriteReg: Function did not return STAT_OK # Error: unable to execute "$L2.5 WriteReg 0xC0 0x44" ERROR - USB communication timed out # WriteReg: Function did not return STAT_OK # Error: unable to execute "$L2.5 WriteReg 0x4C4 0x196e6a" ERROR - USB communication timed out # WriteReg: Function did not return STAT_OK # Error: unable to execute "$L2.5 WriteReg 0xCC4 0" ERROR - USB communication timed out # WriteReg: Function did not return STAT_OK # Error: unable to execute "$L2.5 WriteReg 0xCD0 0x3c0" ERROR - USB communication timed out # WriteReg: Function did not return STAT_OK # Error: unable to execute "$L2.5 WriteReg 0xCC8 0x1" ERROR - USB communication timed out # WriteReg: Function did not return STAT_OK # Error: unable to execute "$L2.5 WriteReg 0xCCC 0x1" ERROR - USB communication timed out # WriteReg: Function did not return STAT_OK # Error: unable to execute "$L2.5 WriteReg 0xCD8 0x105" ERROR - USB communication timed out # WriteReg: Function did not return STAT_OK # Error: unable to execute "$L2.5 WriteReg 0x500 0x0" ERROR - USB communication timed out # WriteReg: Function did not return STAT_OK # Error: unable to execute "$L2.5 WriteReg 0xCD4 0x6000" ERROR - USB communication timed out # ExecutePassthroughDLPAPI: Function did not return STAT_OK # Error: unable to execute "$L2.5 ExecutePassthroughDLPAPI _EnablePwmSeq" ERROR - USB communication timed out # LC_DLP_Source_SetDataSource: Function did not return STAT_OK # Error: unable to execute "$L2.5 DLP_Source_SetDataSource 3" ERROR - USB communication timed out # LC_DLP_Trigger_SetExternalTriggerEdge: Function did not return STAT_OK # Error: unable to execute "$L2.5 DLP_Trigger_SetExternalTriggerEdge 1" ERROR - USB communication timed out # LC_DLP_Display_HorizontalFlip: Function did not return STAT_OK # Error: unable to execute "$L2.5 DLP_Display_HorizontalFlip 1" ERROR - USB communication timed out # LC_DLP_Display_VerticalFlip: Function did not return STAT_OK # Error: unable to execute "$L2.5 DLP_Display_VerticalFlip 0" ERROR - USB communication timed out # LC_DLP_Display_SetDegammaEnable: Function did not return STAT_OK # Error: unable to execute "$L2.5 DLP_Display_SetDegammaEnable 0" ERROR - USB communication timed out # LC_DLP_LED_SetLEDEnable: Function did not return STAT_OK # Error: unable to execute "$L2.5 DLP_LED_SetLEDEnable 0, 0" ERROR - USB communication timed out # LC_DLP_LED_SetLEDEnable: Function did not return STAT_OK # Error: unable to execute "$L2.5 DLP_LED_SetLEDEnable 1, 1" ERROR - USB communication timed out # LC_DLP_LED_SetLEDEnable: Function did not return STAT_OK # Error: unable to execute "$L2.5 DLP_LED_SetLEDEnable 2, 0" ERROR - USB communication timed out # LC_DLP_LED_SetLEDEnable: Function did not return STAT_OK # Error: unable to execute "$L2.5 DLP_LED_SetLEDEnable 3, 0" ERROR - USB communication timed out $L2.5 DLP_LED_SetLEDintensity 0, 50.0 ERROR - USB communication timed out $L2.5 DLP_LED_SetLEDintensity 1, 50.0 ERROR - USB communication timed out $L2.5 DLP_LED_SetLEDintensity 2, 50.0 ERROR - USB communication timed out $L2.5 DLP_LED_SetLEDintensity 3, 50.0 ERROR - USB communication timed out # WriteSYNC: Function did not return STAT_OK # Error: unable to execute "$L2.5 WriteSYNC 1, 1, 0, 0, 1" ERROR - USB communication timed out # WriteSYNC: Function did not return STAT_OK # Error: unable to execute "$L2.5 WriteSYNC 2, 1, 0, 0, 1" ERROR - USB communication timed out # WriteSYNC: Function did not return STAT_OK # Error: unable to execute "$L2.5 WriteSYNC 3, 1, 0, 0, 1" # LC_DLP_Status_GetSeqDataMode: Function did not return STAT_OK # Error: unable to execute "$L2.5 DLP_TPG_SetTestPattern 0, 0, 7, 1" #================================================================= # Downloads images using USB/SPI to external memory (DDR) Commands #================================================================= ERROR - USB communication timed out # WriteExternalImage: Function did not return STAT_OK # Error: unable to execute "$L2.5 WriteExternalImage "C:\Documents and Settings\Dragon\My Documents\LightCommander Control\NewProject3\Solutions\New Solution\Images\dxctest1.dbi", 0" #================================================================= # Write Image Order Table Command #================================================================= ERROR - USB communication timed out # LC_DLP_RegIO_WriteImageOrderLut: Function did not return STAT_OK # Error: unable to execute "$L2.5 DLP_RegIO_WriteImageOrderLut 1, 0" ERROR - USB communication timed out ERROR: could not reset PATLUT index to 0! # LC_DLP_Display_DisplayPatternAutoStepRepeatForMultiplePasses: Function did not return STAT_OK
i'm using the newest software & hardware-firmware version
can you tell me where does the problem occur ?
i hope you give me some advice about it .
Thank you ~~