This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP projector based on LED light source

can any one give me the explanation or any source of information regarding the DLP optical structure based on LED

  • Hi Abel,

    Thanks for your participation on the E2E Community Site.  Which DLP platform are you using?  Discovery 4100?  if so, I can point you to some documentation that should cover the requested information.  For the Discovery 4100, there is an S2+ Optics Module available that has an option for LED based or without an LED.  If you have an external light source that uses fiber optic, an optics adapter for the S2+ can be purchased as well. 

    Once I hear back from you, i will point you in the right direction.  This will help avoid any confusion becuase I don't want to refer you to a resource that does not properly address your questions.

    Regards,

    Justin Lemon

    jlemon@dlinnovations.com