Dear All:
Hi!
We have upgraded the LightCrafter device with latest firmware package 1.1.
But we later found that our previously composed program fail to command the device in Pattern Sequence mode.
We are using command Pattern Sequence Setting (0x40 0x00) to send command, but the device did not respond to the command, which actually works in the previous firmware.
We have also tested the Pattern Sequence feature using the previous version GUI -- Version3.7, and it also failed to give get or set command in that feature, just like what happened in our program.
So we suspect that there might be some back compatible issue of Pattern Sequence in your new firmware package.
Since it works in the new GUI -- Version3.8, we thought that is because you are using command Extended Pattern Sequence Setting (0x04 0x80).
Please take a look at this issue. Thank you!