It's not too clear from the documentation, but what is the best way to reset a pattern sequence? That is, set the "current" pattern to 0.
One way to do this is to "stop" then "start" the sequence, but that seems to add a bit of lag (at least when I do this from the GUI). Another way is to change to static image mode, then back to pattern sequence mode but that seems a bit kludgy... is there a better way to do this?
From the documentation it seems like 0x83 might be related to this, but I'm not sure if that's the intended purpose of this command...