This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About D4100 kit running under the XP mode of Win 7



Hello,everybody. I am using D4100 kit in my system and running  the D4100 explorer in the XP Mode(Win XP SP2) of Win 7 because my whole system is required to run in Win 7 and    
I noticed that somebody in this forum has reported success of such method. But I is very difficult for me to connect the DMD mainboard with my host computer . Even if the moment when they can connect, every time I tried to load data into the board , the D4100 explorer just reports errors and dies with no responding. Now the problem seems to be the USB connection but I don't know how to deal with it. I am wondering  if there is someone who has done this before can help me. 
 Thank you very much.