Is it possible to remove the LEDs and the optics so that I can get light from an external source into and out of the DMD? This system is really affordable and seems to be an ideal way for me to set up a basic single-pixel camera. I do not want the LEDs or associated optics in the light engine, but there is not a simple development kit available at such a low cost without it. Can I buy this simple model and just remove the light engine? Will the DMD still work?