Hello,
To make things easier for our artists, I created a small GUI utility to replace the splash screens, and I'm now looking to implement a button to upload the new binary to the LightCrafter. From the "Command Interface Guide" documentation, it appears 0x07 is the way to go for this.
However, I have questions on how exactly 0x07 is meant to be used before I accidentally brick the LCr!
1) Byte 4 to Byte 35 -- does this string require a specific format for the version number? Or can it be anything?
2) 37-39 are reserved. Can I just put 0 into these bytes for the write payload?
3) 80-83 is the 32bit checksum of the first file... what algorithm should be used to calculate the checksum? Just add up all the bytes in the bin file?