What is nominal principal point of LightCrafter?
I'm trying to calibrate it as a pin hole camera model.
Due to the Offset of 100%, It doesn't seem to be at the center of the image.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is nominal principal point of LightCrafter?
I'm trying to calibrate it as a pin hole camera model.
Due to the Offset of 100%, It doesn't seem to be at the center of the image.
Sean,
The LightCrafter light engine has what is called a 100% offset. The height of the DLP3000 array is 3.7 mm. That means that the principal point is 1.85 mm above the center of the DMD array.
NOTE: I edited this response to correct an error in my answer. I had assumed that 100% offset would result from moving the array its full height away from the principal point. I have been corrected on this assumption by one of our optical experts. 100% offset means that the DMD array is moved by half its height. Sorry for the confusion.