Hello
I was trying to use d4000_usb.dll to control dmd in c++.
I use a DLP-4100 Controller Board.
Usually, I can load data by using the LoadToDMD function,
But sometimes this function receive no reply, and than my program used by d4000_usb.dll (Build 2008/11/13) was halt or hold.
If you have a newly version(D4000_usb.dll) or patch version, Please could you give me a that?
Thank you in advance!