I have a .55" XGA Type X mirror. Because of the default row loading order, it will be simpler to use one of the sides of the DMD as the top of my image. Is it safe to mount the DMD so the screen is in the "portrait" position instead of the normal "landscape" position? Will this affect the mirror tilt angles or provide more strain on the mirrors or other DMD parts?