Dear Sir/Madam,
I am planning to buy a DLP Pico Projector Development Kit 2.0 for using in my project. I would like to know if the projector will be compatible with the system specifications that I plan to use. I will be working on a laptop that has: HDMI port, 15-pin VGA port, Ubuntu 12.04 (Linux 64-bit OS), Screen Resolution (Min - 800x600, Max - 1366x768), Display Card - ATI Mobility Radeon HD 4500 Series.
If any other information is required, I would be glad to provide the same.