Is there any way to have true black with the Lightcrafter? The "black" I see is still too bright.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there any way to have true black with the Lightcrafter? The "black" I see is still too bright.
Tyler,
The difference between the brightest white, and the blackest black is the contrast ratio of a projector. This is dependent upon several factors: 1) DLP DMD characteristics; 2) System optics (illumination and projection) design; 3) Light Engine materials and construction; 4) Light Engine alignment; 5) Ambient lighting conditions
The DLP3000 uses the same DLP technology which is noted for excellent (industry leading) contrast ratio. The light engine supplied with the DLP LIghtCrafter is a well designed and executed Pico projetor light engine - but remember that it is a cost/performance compromise. A specially designed, specified, carefully built - and very expensive - light engine would probably provide a higher contrast ratio.
Have you tried setting both a solid white pattern - then a solid black pattern? Those are available in the LightCrafter GUI under Internal Test Patterns.
I have used a solid black test pattern, but unfortunately that is still too bright. I am using a reflected image, and I can see the scattered light from the micromirrors thus obscuring the background. I have thought of using layers of filters and setting the image to be very bright. Perhaps that will get rid of the scattered light while allowing the image I want superimposed through.
Perhaps the LEDs for the projector are just too bright for my application, even when I use the software to dim the LED output. Maybe I need a dimmer LED output. Hmmmm....
Thanks again Pascal. It seems you're always helping me here.