Hello,
I would like to be able to control the mirror array from an external DSP. Ideally, the DSP would determine the bitmap that should be applied to the bitmap in real time and send it to the Lightcrafter at 1 kHz (rates up to say 10 times slower would be acceptable). Is there any way to achieve this, perhaps through the pattern sequence mode? If not, would there be a way to load to say 60 bitmaps into the Lightcrafter and control which one should be applied from the DSP (at the same ideal frequency of 1 kHz)?
Thank you,
Albert Wildeman