Hi
We are planning to use DMD Discovery 1100 for 355 nm laser. In the data sheet it says max power for dmd 1100 is 0.1 W/cm^2 for wavelength<350nm. But the laser we use will have the power ~5 W/cm^2. Does it mean DMD 1100 won't apply in our process?
Also the data sheet only has reflectivity for 420~700nm. What will be the reflectivity( or transmission) for 355nm? Because we need to calculate the loss to see if it's acceptable.
Thanks!