I put a probe on the TP12, TP13 and TP14 points, expecting to see a PWM signal, but instead just got 3.1V on TP12/TP14 and nothing on TP13. Is this correct? Also, does the light engine use shutters in front of the LED's and if so, is there a way to control them?