This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using extended pattern sequence from programming languages like MATLAB

I have been trying to use the extended pattern sequence from MATLAB. However, I have not been able to use (0x04 0x81) from MATLAB to upload the images although I can use the extended pattern sequence from the GUI. Moreover, I have checked the extended pattern sequence settings and they seem to be set correctly . In this regard, I have a few questions.

First, it seems that counting of patterns starts at 0; however, I am not clear about the number of patterns that can be loaded as in the Command Interface Guide the range of patterns is given as 1-1000 under the description of command 0x04 0x80 whereas the range of pattern number is given as 0-1500 under the description of 0x04 0x81. 

Second, what is the range of row and column numbers? Expressed in other words, if I want to use all of the DLP should my column and row numbers be 0x00 0x00 or 0x01 0x00.

Third, since I have been uploading images for pattern sequence from MATLAB without any problem, it would be helpful to know if there is any significant difference in using 0x04 0x81 versus 0x04 0x01 as far as loading images is concerned. 

Any and all information on the topic will be highly useful. Thanks.