Hello,
I'm using the lightcrafter in 1 bit 1 color mode over HDMI to project patterns at 1440 Hz. However, I notice that between each frame (i.e. after every 24 patterns) there is a roughly 400 microsecond delay before the next frame starts (measuring the output light with a photodiode). Moreover, it seems that all mirrors turn "off" during this 400 microseconds regardless of the settings in the previous frame.
Is there any way to eliminate this 400 microsecond delay or at least have the lightcrafter continue displaying the previous pattern during the delay?
Thank you!