Dear Forum,
Thanks for a very organized forum!
I think I managed to break the capacitor C60 when I removed the Light Engine :-(. Does anyone know the specifications of capacitor C60? It is located at the lower board on Lighcrafter next to one of the two screws that holds the small vertical green board on to which the DMD sit.
For other people who wants to remove the light engine: I would suggest a small adjustement to the "LighEngine" description in this forum.
Unscrew not only light engine from base plate, but also both boards. Then one can just pull out the light engine (given that both ribbons are disconnected!). Once this is done there is no C60 in the way for the screw, and that screw can be easily and safely removed.
Best regards,
David