Im trying to test some DLP projectors which apparently have 3D capabilities via VGA input. Anyone out there have a link to a 3D image for inputting into a DLP projector via VGA? Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Im trying to test some DLP projectors which apparently have 3D capabilities via VGA input. Anyone out there have a link to a 3D image for inputting into a DLP projector via VGA? Thanks
Hello again Daniel,
Here is what I have learned from our team here. You need to set the projector to 120Hz using a compatible video card (Nvidia Quattro is a good example).
Then go find 3D content. 3D is "movies", not "images"; even if the "movie" only shows a static image. This is because it shows two frames L/R so the projector handles it as a movie.
You can Google "stereoscopic" player (example http://www.3dtv.at). Many other (free) online content sources are available (i.e. youtube). There are also tools for creaation. 3DTV also has sample source movies available for free download.
Fizix