Hi,
I am asking what exactly is stored in the spi flash of the dlpc300. Is it firmware code? Non-volatile parameters?
Does the read interface on the spi expected data immediately or is it a posted read?
What I'm try to figure out is do I need a separate SPI flash for the dlpc300 or can I use the flash connected to my processor and use a SPI interface inside of my fpga to connect to the dlpc300. My fpga is a soc arm processor included chip.
Thanks,
Elaine