Other Parts Discussed in Thread: DLPC200
Hi,
I'm new here and trying to obtain 1000 fps binary display with dlpc200. I need to synchronize each binary pattern to the corresponding sample position.
After I went through various threads here, I may have two option to obtain my goal. One is to download all binary patterns to the memory and execute it by calling LUT. This is the only way to achieve the highest frame rate and pattern sync, but we need to download every 1000 images whenever the image sets should be changed. Every single binary pattern will be different and I may have to download after 1000 patterns are displayed. I read some answers that the download is not fast compared to the frame rate. Is this correct?
The second method would be the structure light mode via DVI with packing 20 bits to one frame and running the dmd with 50 fps. I think I should go this method, but I wonder the each bit plane (among 1000 bit planes) has same on time like 1 ms? The binary weighting is not applied to the structure light mode? I also want to know if there is a way to sync each bit plane in this mode.
Thank you.
Yun-Ho