This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Issue with output trigger after upgrade to 2.01 buddle



After I upgraded to 2.01 bundle (leaving MSP430 at v.2.5 since I removed light engine), the output trigger got stuck at 30Hz regardless of the mode (hdmi, internal patterns, pattern sequences, static images etc.).

I had to downgrade to older version (DM365 3.31, FPGA 2.4.39, MSP430 2.5) to get the output trigger to work again.

Could you please verify this? Thanks!

  • Hi Bing,

    Thanks for informing us about the output trigger problem. We have verified that Output trigger freezes at 30 Hz but it's inconsistent. We need to investigate the issue further and will provide an update as we progress.

    Regards,

    Divya