Hi,
A problem comes up when I use the LCr to trigger a Imaging source camera 31Bu03. The triggering can fail occasionally.
Settings:
exposure time: 16667us for both the camera and Lcr
output trigger pulse width: 100us
the system board change has been made according to the guide, but the voltage between pin1 and pin3 of J7 is measured at 3.18V instead of 3.3V. The process ( Lcr projects--trigger--camera snaps) runs smoothly most of the time, but sometime it gets stucked. Howerver, if I break one of the cable (e.g. the one connecting the Pin1 of J7 and the center conductor of the BNC jack ) and connect it again, it runs correctly again. It seems that the camera hasn't been triggered properly becasue there's no trigger signal, but i have no device to detect the LightCrafter's output trigger.
I'm sure the cable connection is ok. So what causes this? Is it guaranteed that if the command successes, the LCr will give a trigger singal? Or it's just because the voltage isn't enough? if so , why it works most of the times as well as manually cause a signal(mentioned above)? Someone gives me some help please. Thanks