This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMD1000 problem

dear all

Resently  I  meet a   problem like this:

The system  is based DDP3021, and there is a  PMD1000 power chip.  

Its voltage range is from 10.8V to 13.2V.  

Normally the input  voltage is 12V.

The problem is : when the  input  voltage is  bigger than  11.7V,   the pwrgood signal is not  pulled to high level.

When the voltage is reduced to 11.7V or lower , the pwrgood is ok.

Is there any solution ?

thanks!