Hi all,
so far I got no reply to my inquiry concerning the level of noisiness of the cooling fan on the DLP LightCrafter 4500, and I figure it is not obvious to quantify, so I'll try to be more specific with my questions:
- can you hear the fan at all in a silent surrounding when you switch on the device?
- (this for the TI engineers) if necessary can you unplug/disable the fan when using the LEDs at lower currents, eg for light intensities comparable to the original DLP Lighcrafter (the one with no active cooling), or is this not recommended because of a different arrangements of the LEDs/heat sinks in the newer device?
Any insight on these topics would be very welcome!
Zuzanna