Hi,
I think its great that the lightcrafter 4500 can operate without a computer. One drawback is the image load time. I mean the time thats its needed to load an image from the flash memory into the buffer.
My question is: when developing a custom board for controlling that DMD would it be possible to add additional RAM or something like that to load the images from that into the buffer instead from the flash? I want to avoid the image load time.
C.