This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to make 1440 (60*24) pattern in lightcrfater?

Other Parts Discussed in Thread: DLPC300

Hi.

I have question about making 1440 (60*24) pattern via hdmi video.

Theoretically, I can understand that 24patterns consists 1 frame when selecting 1bit mode.

So I tried make 1440fps video (avi) and then play it via hdmi video, but I couldn`t find 1440HZ  by photodetector.

There is just 60HZ measured by photodetector. I tried 720fps video, the result was same.

Also I tried to make video file using tiff image file which is made by ' imageJ' program. I made tiff file with 24 slide, and  then make video file with these tiff file. But the result was same. I couldn`t find 1440HZ.

What can I do?

The video file output was 16bit YUY2 type. Is this make problem?

or Is there any idea to make 1440 HZ pattern?

Any idea would be appreciated. thanks.

Best regards,

Lee.D.H.