Hi,
I tried to use SD card to boot for LCr, because LCr failed at 95% process bar with Nand flash boot.
Attached is the log of boot messages from SD card boot.
Please give me some suggestions.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sanjeev,
Thanks for your reply.
Attached is the printscreen which copying SD boot image into SD Card(4GB size) from DLPlightcrafterSoftwareBundle-2.0.1.
I supposed when boot from SD succeed, the version of DM365/MSP430/FBGA is latest.
Thanks.
Hi Leomon,
Sorry, from your earlier discussion, I understood you are able to update and boot your system. Is it not the case?
Are you still facing the problem of failed to boot after showing 95% even with 4GB SD card?
One more suggestion, you can do a clean format of the disk using HP USB Disk Storage Format tool, and they try loading the software again. On Windows 7 platform you need to run the tool as admin.
Regards,
Sanjeev
Hi Sanjeev,
Yes, I still have problem with boot issue on NAND flash or 4GB SD card.
Sometimes, LCr can boot successfully once , then I can get the version of DM365,FPGA, MSP; but it cannot boot by SD card.
Could you help explain the debug log(failure message) from SD boot that I provided for you.
Thanks.
Hello Leomon,
You meant the booting worked once but not consistenly. Most of time it fails to boot either from SD card or NAND flash.
Is that correct?
Here is the reason -
In the LightCrafer DM365 for SD Card flash and booting the software is taken from here http://processors.wiki.ti.com/index.php/SD_card_boot_and_flashing_tool_for_DM355_and_DM365 we have identified issue where the software is stuck while initializing the SD card.
The fix for this issue will be made available in the upcoming release DM365 v5.0.0. We'll be releasing in next couple of weeks.
Let me know if anything I can helpful at this point of time.
Regards,
Sanjeev
Hi Sanjeev,
Yes, you are correct.
But I still don't understand why this LCr can boot successfully once but not consistently.
And if upgrading the DM365 software version5.0.0 into Nand flash, whether the booting issue can be solved.
Thanks.