This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Programming Interface for LightCrafter 4500

Other Parts Discussed in Thread: DLPC350

Hi all,

I'm setting up the LightCrafter 4500 to be used for medical research purposes, and the color space conversion and degamma settings need to be turned off, so that we know exactly what the light intensity is at every point, but we still want to have temporal multiplexing, so that the image appears continuous.  I believe the only way to do this is through the programming interface.

I'm having a lot of issues trying to run the LCR 4500 in the programming interface.  I was using the example code I found in the forums, but it seems like it's only compatible with the LCR 3000.  Is there a way to modify the LCR 3000 programming interface code to be compatible with the LCR 4500?  I can't find much information about connecting the LCR 4500 through anything but the GUI (which is working, just not what we need).

Thanks,

Sydney