This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I2C Issue

Other Parts Discussed in Thread: DLPC300

I'm a stranger on English

Hi... I make circuit using dlpc300.

I have a trouble, that's dlpc300 don't send ack.

I check flag(INT4.) and send data.

I attach 2 files.

One is Light Craft 2.0's image, and the other is my board's image.

I know that clock's first low period is different. But I could use this on DLP PICO PROJECTOR.(address etc. are different.)

---------------------------------------------------------------------------------

I answer one more question.

When DLPC300 make a pulse(flag on INT4), can I think DLPC300 is no problem?

Is there time limit on I2C after flag?