Hello,
When it is projected to be set to 10ms from 8.3ms the Exposure Time,
and outputs the data written to the internal buffer 0 of DLPC300,
enable signal to the LED is output shorter than the set time.
Time that is shorter is about 150us.
This enables the difference between the exposure time of the camera,
correct image can not be captured.
Enable is output in a normal period of time data output of 1-3 buffer
and the other without problems, without changing the Exposure Time,
Reading the buffer 0 again.
(It seems to be only funny the first projection after the setting change).
Be considered as What is the cause?
DMD has been used in 8bit monochrome mode.
In addition, not only the 8.3ms → 10ms, it will occur only when
the setting Exposure time is longer in the Internal Mode and 10ms → 12ms.
Frequency of occurrence is 100%.
Best regards, RY