This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

display multiple images with multiple exposure time



Hello,

In our application, we need to project multiple images and each image has its individual exposure time. I don't want to use static image mode because of gamma correction. However, in sequence display mode, I have to specify the exposure time, which is the same for all frames. So my question is, is it possible that I can control how long the display the image without pre-determined exposure time. 

Thanks!

  • You can create multiple bit depth and multiple color pattern sequences following this app note. But all patterns must have the same exposure time and this must be known to create the pattern sequence. You can use this multi-bit/multi-color approach using the minimum exposure time and have some patterns duplicated to simulate larger exposure times.