Hello all and thanks for the help,
I have two Light Crafter 2.0. In the old one I am able to load a certain number of images and is working perfect (it has an old version 2.0.1 ).
With the new one I have some problems. After the upgrade to the version 2.0.1 I found out that for certain number of images I got a command error - packet failed. So I decided to upgrade this to the version 3.0 but still I have the same problem.
I also notice that in the drop down button list seems that you can just load even number of images after 25. In fact with 25-27 and others I have my packet fail error.
I wondering why, because with the other LCr I don't have this issue at all.
Thanks for your help.
Pablo