Hi,
I want to use DMDs for optical communication, where a single mirror will represent a single communication channel. For this purpose I need to load a static image to DMD which sometimes can be changed (once a day/week ). I am looking for a simple DMD control circuitry which would be suitable for this application.
I could use LightCrafter but since I need to control more than 300 DMDs the option to use 300 LCs is not affordable.
I would like to understand:
1) does the simple circuit for static image loading exist? what are the minimum requirements?
2) is it possible to use one LightCrafter to run 300 DMDs displaying static images?
Thank you
Alex