This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Enabling the RNDIS driver on Ubuntu

Other Parts Discussed in Thread: DLPC350

Hi,


I'm trying to connect DLP Lightcrafter 4500 with a PC running Ubuntu 12.04. I'm following the instructions in DLP Lightcrafter EVM Users Guide but I'm unable to assign the ip address to usb0. I use the following command:

sudo ifconfig usb0 192.168.1.99 up

which returns

SIOCSIFADDR: No such device
usb0: ERROR while getting interface flags: No such device
usb0: ERROR while getting interface flags: No such device

Has this been previously experienced? I'm not sure what the problem is so I would appreciate if anyone has suggestions.

Thanks


Thanks