hi,
I have the DLP 5500 connected to an external light source. I have created 8 bit gray scale patterned images (sinusoidal) to be projected on a sample.
Recently I have noticed problems with my DLP projecting true gray scale patterns. I am using the PD logic DLP control software to import 8 bit patterned images. I have noticed that the patterns coming out of the DLP are not exactly 8 bit; I see dark lines in between one shade and another in the same image and these lines will change according to LED illumination time. Note that I am not using the LEDs connected to the DLP, but rather have a Lumencore light source (other LEDs) connected. I cannot disable this. I project one pattern and capture it with 14 bit CCD. I have tried syncing with an external 3V source, but still get the same effect. I have played with the frame rate as well and the software sometimes does not allow for high frame rate even though I choose frequencies below the maximum allowed frequency. Would you know what is happening and why I get the lines in between gray intensities? What can I do? Help please!