This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DMD controller board for DLP4500NIR

Other Parts Discussed in Thread: DLP4500NIR, DLP4500, DLPC350

Can the DMD controller board of the DLP4500 LightCrafter reliably control a DLP4500NIR?


I am looking into a reliable way to control DLP4500NIR to spatially modulate 790nm light in a custom built confocal microscope.  The question is on whether acquiring a DLP4500 LightCrafter, removing the controller board and then connect it to a DLP4500NIR will work.


Thanks,

Andres

  • Hello Andres,

    Yes, the controller board should be able to talk to DLP4500NIR without any problems. All you need to do is replace DLP4500 with DLP4500NIR chip. 

    The DLP4500NIR is fully compatible with DLPC350 controller sitting on the DLP4500 LightCrafter controller board.

    Regards,
    Sanjeev