I use the LightCrafter to develop an application with its DLP3000. The light engine has been removed. I intend to use white light generated by a halogen tungsten lamp to illuminate the DMD chip, and use the DMD as a group of mirrors that can be controlled via programming. However I found that there is dispersion problem. The reflected light seems to be colorful. Is it related to the angle of the incident light? How can this problem can be solved? Is it possible to use white light as the source? Thanks.