Hello E2E,
I am having the exact same problem as posted by user Houman Kamran from this thread: http://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/850/t/176873.aspx?pi201799=1
I was also lead to this problem in the exact same way as this user. I desperately need pattern sequence to work and some threads I came across were successful in getting pattern sequence to work by simply upgrading the firmware and software to the latest versions.
Again, I did the upgrade exactly as this thread, the upgrade video, and the manual says to; with successful writing of the image file to the SD card whether I tried from the nand or sd. Houman says he got it to work finally by just turning the LightCrafter off from the driver board and on again after about a 5 second delay. However, this still does not work for me. I am getting very frustrated that the LightCrafter will still not boot after many times of trying directions verbatim.
Another piece of info is that when I try for a boot up, sometimes the splash display is somewhat more blurry than other times.
I am using a Kingston 4GB microSD and am on a Windows 7 machine.
Thanks in advance for any help. This is a cool little gadget and I would love to get it to work.