The DLPC350 is expensive,and I want to use an general ARM9 to control the DMD for my Independent-design spectrometer.I means that it can avoid use two proccesor.And the DLPC350 's core is ARM9,isn't it?
1.What‘s the difference between ARM9 and DLPC350?DLPC350's kernel is ARM9 ,isn't it?
2.what‘s DLPC350 programming process ?
3.Can use an ARM9 to control the DLP4500NIR?
4.How to control the DMD?do you have some program to control the DLP4500NIR example?
please!