Hi,
I have bought the DLP4500 and i'm using a red laser as a light source. The problem is that there are diffraction just as seen in the "Using lasers w/ DLP DMD Technology". The result I want to have is to have only a single order illuminated the most so that at a considerable distance from the mirror only 1 laser dot is seen.
After reading that information and other stuff, i got some questions:
1) in reference to the Littrow configuration (alpha=beta=blazed angle) and having fixed grating pitch and mirror tilt, should I be choosing laser wavelength that is best for this mirror since the blaze angle is the mirror tilt angle? and will this do the job?
2) It was written in the earlier note that "it is possible to move the incident angle to arrange a blaze for a given (n,n) order." How is this optimal incident angle found (say for 1st order) knowing that mirrors tilts 12 degrees, given a particular wavelength ?
3) (cont in Q2) if incident light is at this particular angle where it's blaze is for a given order, will the diffraction at other oder not be seen at a close distance to the mirror OR will it be seen at close distance the mirror but not at further distance?