Hi
I've tried to use Lightcrafter pattern sequence mode to project b/w patterns. But I can use only one color LED at once.
Questions a) Can I use MBMC Sequence Settings to project b/w patterns through pattern sequence settings?
b) If a) is possible, what is the correct pattern sequence?
b-1) Exposure time : 250us (as low as possible) Pattern : 1bppX1R_1bppX1G_1bppX1B_250us
b-2) Is limitation of the total number of bit planes(96) restricts the total number of the pattern images?
b-3) If b-1) is possible, flicker can occurs?
c) If a) is impossible, is there any other solution to use pattern sequence mode to project b/w patterns?
Regards
HSKim