Hi,
I want to use external pattern sequences mode but I am not sure how?
The LIightcrafter 3000 is connected to PC and HDMI has been pluged in.
Then when I use HDMI port mode and change the mode from RGB Video to extenal streaming pattern, there seems no difference, just projecting PC's screen.
Should I use FPGA(with HDMI output) or GPU or sth.else to store patterns and then make program to transfer patterns to Lightcrafter in high speed so that I can use the external pattern sequences mode? Really confusing and frustrated.
More, I read some other response related with external patterns mode and they mentioned several command such as 0x00,0x80,0x40. I do not find them on the GUI. What are they used for?
Please help me ! TAT
Thanks and regards,
William