This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NED with LightCrafter EVM



I have recently purchased the LightCrafter Display 2010 EVM. I am looking to convert this type of system into a near eye display. The current state of the EVM is too large for my needs; however if the optical driver could be separated (or bought separately) then the size of the PCBs on the EVM would not be a problem for my application. I am curious if anyone know this these components could be separated and if so is it possible to attach the optical driver to the rest of the EVM with cables ~1 m in length.


Thank You,
Dylan Matteson