Hey,
I have been working on the NIRscan EVM for a while now. We only have the main board and the DMD attached to it, since we don't need any of the other components. For my research purposes I need to be able to insert BMP images into the framebuffer at a rate of about 1 per second.
When browsing through the dlp_nirscan source code I noticed it can load BMP images into the DLPC350 framebuffer using ioctl commands. I find these commands very hard to follow and I wonder if there is any documentation on how the images are loaded into the framebuffer.
I hope some light can be shed on this.
With kind regards,
Gordian