Hi all,
I apologize if this is the incorrect forum, but I can't find one specific to questions about DMD components.
My question is regarding the 0.3 WVGA EM DDR Series 242 DMD.
The absolute maximum temperature rating is listed as 75C for BOTH a reference location (TC1) on the ceramic package AND the active array. How is this possible? According to the datasheet, the active array temperature must be calculated as a sum of TC1 and some power produced by the array. Clearly, the active array temperature will always be hotter.
So, is this maximum temperature of 75C referring to the active array, in which case I have to back out a cooler TC1 based on operating conditions? Or does it mean that the active array can be some value hotter than TC1, when TC1 is 75C?
Thanks!
Colin